21.5.12 I/O Lines Lock
When an I/O line is controlled by a peripheral (particularly the Pulse Width Modulation Controller PWM), it can become locked by the action of this peripheral via an input of the PIO Controller. When an I/O line is locked, the following fields in PIO_CFGRx/PIO_P_CFGRx are locked and cannot be modified:
- FUNC: Peripheral selection cannot be changed when the corresponding I/O line is locked.
- PUEN: Pull-Up configuration cannot be changed when the corresponding I/O line is locked.
- PDEN: Pull-Down configuration cannot be changed when the corresponding I/O line is locked.
- OPD: Open Drain configuration cannot be changed when the corresponding I/O line is locked.
Writing to one of these fields while the corresponding I/O line is locked will have no effect.
The user can know at anytime which I/O line is locked by reading the PIO Lock Status Register (PIO_LOCKSR) or PIO Privilege Lock Status Register (PIO_P_LOCKSR) for locked Privileged-Access mode I/O lines. Once an I/O line is locked, the only way to unlock it is to apply a hardware reset to the PIO Controller.