1.2.4.4.8 SYS_CONSOLE_Flush Function
C
bool SYS_CONSOLE_Flush(const SYS_CONSOLE_HANDLE handle)Summary
Flushes the read and write queues for the given console instance.
Description
This function flushes the read and write buffers. Any on-going transfers will not be flushed.
Preconditions
The SYS_CONSOLE_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| handle | Handle to the console instance |
Returns
true - If the operation is successful
false - In case of failure
Example
SYS_CONSOLE_HANDLE myConsoleHandle;
bool status;
// myConsoleHandle is assumed to be a valid console handle
status = SYS_CONSOLE_Flush(myConsoleHandle);
if (status == false)
{
// Handle error
}Remarks
This API may do nothing and return true, where the read and write are not buffered.