1.2.4.4.7 SYS_CONSOLE_Write Function
C
ssize_t SYS_CONSOLE_Write(
const SYS_CONSOLE_HANDLE handle,
const void* buf,
size_t count
)Summary
Writes data to the console device.
Description
This function writes data to the console device. The function performs a deep-copy of the data passed in buf.
Preconditions
The SYS_CONSOLE_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| handle | Handle to the console instance |
| buf | Buffer holding the data to be written. |
| count | Number of bytes to write. |
Returns
The return value indicates the number of bytes accepted by the function.
In case the return value is less than the count value, the application must try to send the remaining bytes in next attempt(s).
Returns -1 in case of any error.
Example
ssize_t nr; char myBuffer[] = "message"; SYS_CONSOLE_HANDLE myConsoleHandle; // myConsoleHandle is assumed to be a valid console handle nr = SYS_CONSOLE_Write( myConsoleHandle, myBuffer, strlen(myBuffer) ); if (nr == -1) { // Handle error } if (nr != strlen(myBuffer)) { // Try send the remaining data after some time. }
Remarks
Application may check the free space available in the transmit buffer by calling the SYS_CONSOLE_WriteFreeBufferCountGet() API.