1.2.4.4.5 SYS_CONSOLE_DeviceGet Function
C
SYS_CONSOLE_DEVICE SYS_CONSOLE_DeviceGet( const SYS_CONSOLE_HANDLE handle)Summary
Returns the device type for a given console instance
Description
This function returns the device type supported by the given console instance
Preconditions
The SYS_CONSOLE_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| handle | A valid handle to the console instance |
Returns
SYS_CONSOLE_DEVICE - Returns console device type. Returns SYS_CONSOLE_DEV_MAX in case of an error.
Example
SYS_CONSOLE_HANDLE myConsoleHandle; SYS_CONSOLE_DEVICE myConsoleDevType // myConsoleHandle is assumed to be a valid console handle myConsoleDevType = SYS_CONSOLE_DeviceGet(myConsoleHandle);
Remarks
None.