1.1.8.4.14 DRV_SFDP_GeometryGet Function
1.1.8.4.14 C
bool DRV_SFDP_GeometryGet( const DRV_HANDLE handle, DRV_SFDP_GEOMETRY *geometry );1.1.8.4.14 Summary
Returns the geometry of the device.
1.1.8.4.14 Description
This API gives the following geometrical details of the SFDP Flash discovered at runtime using SFDP:
- Number of Read/Write/Erase Blocks and their size in each region of the device
- Flash block start address.
1.1.8.4.14 Precondition
The DRV_SFDP_Open() routine must have been called for the specified SFDP driver instance.
1.1.8.4.14 Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| *geometry | Pointer to Flash device geometry table instance |
1.1.8.4.14 Returns
True - If able to get the geometry details of the Flash.
False - If SFDP discovery fails or read device id fails.
1.1.8.4.14 Example
DRV_HANDLE handle; // Returned from DRV_SFDP_Open DRV_SFDP_GEOMETRY sfdpFlashGeometry; uint32_t readBlockSize, writeBlockSize, eraseBlockSize; uint32_t nReadBlocks, nReadRegions, totalFlashSize; DRV_SFDP_GeometryGet(handle, &sfdpFlashGeometry); readBlockSize = sfdpFlashGeometry.read_blockSize; nReadBlocks = sfdpFlashGeometry.read_numBlocks; nReadRegions = sfdpFlashGeometry.numReadRegions; writeBlockSize = sfdpFlashGeometry.write_blockSize; eraseBlockSize = sfdpFlashGeometry.erase_blockSize; totalFlashSize = readBlockSize * nReadBlocks * nReadRegions;
1.1.8.4.14 Remarks
This API is more useful when used to interface with Memory driver.