1.1.8.4.11 DRV_SFDP_ReadStatus Function
1.1.8.4.11 C
bool DRV_SFDP_ReadStatus( const DRV_HANDLE handle, void *rx_data, uint32_t rx_data_length );1.1.8.4.11 Summary
Reads the status register of the Flash device.
1.1.8.4.11 Description
This function schedules a blocking operation for reading the Flash device's status register. The status register contains information about the device's current operational state.
1.1.8.4.11 Precondition
The DRV_SFDP_Open() routine must have been called for the specified SFDP driver instance.
1.1.8.4.11 Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| *rx_data | Buffer pointer into which the status register data will be placed |
| rx_data_length | Number of bytes to read from the status register |
1.1.8.4.11 Returns
True - If the status register read is successfully completed.
False - If read status command fails.
1.1.8.4.11 Example
DRV_HANDLE handle; // Returned from DRV_SFDP_Open
uint8_t statusRegister = 0;
if (DRV_SFDP_ReadStatus(handle, (void *)&statusRegister, sizeof(statusRegister)) == false)
{
// Error handling here
}1.1.8.4.11 Remarks
This function can be used to poll the device's ready status or other operational flags.