1.1.8.4.7 DRV_SFDP_SectorErase Function
1.1.8.4.7 C
bool DRV_SFDP_SectorErase( const DRV_HANDLE handle, uint32_t address );1.1.8.4.7 Summary
Erase the sector from the specified block start address.
1.1.8.4.7 Description
This function schedules a non-blocking sector erase operation of Flash memory. The sector size is determined from SFDP discovery (typically 4 KB).
The requesting client should call DRV_SFDP_TransferStatusGet() API to know the current status of the request.
1.1.8.4.7 Preconditions
The DRV_SFDP_Open() routine must have been called for the specified SFDP driver instance.
1.1.8.4.7 Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| address | Block start address from where a sector needs to be erased |
1.1.8.4.7 Returns
True:
- If the erase request is successfully sent to the Flash
False:
- If Write enable fails before sending sector erase command to Flash
- If sector erase command itself fails
1.1.8.4.7 Example
DRV_HANDLE handle; // Returned from DRV_SFDP_Open
uint32_t sectorStart = 0;
if(DRV_SFDP_SectorErase(handle, sectorStart) == false)
{
// Error handling here
}
// Wait for erase to be completed
while(DRV_SFDP_TRANSFER_BUSY == DRV_SFDP_TransferStatusGet(handle));1.1.8.4.7 Remarks
None.