DRV_MX25L_PageWrite Function
C
bool DRV_MX25L_PageWrite( const DRV_HANDLE handle, void *tx_data, uint32_t tx_data_length, uint32_t address );
Summary
Writes one page of data starting at the specified address.
Description
This function schedules a non-blocking write operation for writing maximum one page of data into Flash memory.
The requesting client should call DRV_MX25L_TransferStatusGet() API to know the current status of the request.
The request is sent in QUAD_MODE to Flash device.
Preconditions
The DRV_MX25L_Open() routine must have been called for the specified MX25L driver instance. The Flash address location which has to be written, must have been erased before using the MX25L_xxxErase() routine. The Flash address has to be a Page aligned address.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| *tx_data | The source buffer containing data to be programmed into MX25L Flash |
| tx_data_length | Total number of bytes to be written. should not be greater than page size |
| address | Write memory start address from where the data should be written |
Returns
True:
- if the write request is successfully sent to the Flash
False:
- if Write enable fails before sending sector erase command to Flash
- if write command itself fails
Example
#define PAGE_SIZE 256 #define BUFFER_SIZE 1024 #define MEM_ADDRESS 0x0 DRV_HANDLE handle; // Returned from DRV_MX25L_Open uint8_t CACHE_ALIGN writeBuffer[BUFFER_SIZE]; bool status = false; if(DRV_MX25L_SectorErase(handle) == false) { // Error handling here } // Wait for erase to be completed while(DRV_MX25L_TransferStatusGet(handle) == DRV_MX25L_TRANSFER_BUSY); for (uint32_t j = 0; j < BUFFER_SIZE; j += PAGE_SIZE) { if (DRV_MX25L_PageWrite(handle, (void *)&writeBuffer[j], (MEM_ADDRESS + j)) == false) { status = false; break; } // Wait for write to be completed while(DRV_MX25L_TransferStatusGet(handle) == DRV_MX25L_TRANSFER_BUSY); status = true; } if(status == false) { // Error handling here }
Remarks
This routine will block wait until write request is submitted successfully.
Client should wait until write is complete to send next transfer request.