DRV_MX25L_ReadJedecId Function

C

bool DRV_MX25L_ReadJedecId( const DRV_HANDLE handle, void *jedec_id );

Summary

Reads JEDEC-ID of the Flash device.

Description

This function schedules a blocking operation for reading the JEDEC-ID. This information can be used to get the Flash device geometry.

The request is sent in QUAD_MODE to Flash device.

Precondition

The DRV_MX25L_Open() routine must have been called for the specified MX25L driver instance.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open routine

Returns

True - If the read is successfully completed.

False - If read jedec-id command fails.

Example

DRV_HANDLE handle; // Returned from DRV_MX25L_Open
uint32_t jedec_id = 0;

if(DRV_MX25L_ReadJedecId(handle, &jedec_id) == false)
{
    // Error handling here
}

Remarks

This routine will block wait for transfer to complete.