DRV_MX25L_TransferStatusGet Function

C

DRV_MX25L_TRANSFER_STATUS DRV_MX25L_TransferStatusGet( const DRV_HANDLE handle );

Summary

Gets the current status of the transfer request.

Description

This routine gets the current status of the transfer request. The application must use this routine where the status of a scheduled request needs to be polled on.

Preconditions

The DRV_MX25L_Open() routine must have been called for the specified MX25L driver instance.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open routine

Returns

DRV_MX25L_TRANSFER_ERROR_UNKNOWN - If the Flash status register read request fails.

DRV_MX25L_TRANSFER_BUSY - If the current transfer request is still being processed.

DRV_MX25L_TRANSFER_COMPLETED - If the transfer request is completed.

Example

DRV_HANDLE handle; // Returned from DRV_MX25L_Open

if (DRV_MX25L_TransferStatusGet(handle) == DRV_MX25L_TRANSFER_COMPLETED)
{
    // Operation Done
}

Remarks

This routine will block for hardware access.