2.6 Adding and Configuring G3 Stack to Project

  1. Add G3 Stack Component. On Device Resources, navigate to SmartEnergy>G3 Stack and click the + sign next to G3 Stack.
    Figure 2-24. Add G3 Stack
  2. Double click the G3 Stack folder just added, or select G3 STACK on the View Selector in Project Graph window. This opens a new Project Graph view, where G3 Stack components will be added and configured.
    Figure 2-25. Select G3 Stack
  3. Configure G3 Stack Component.
    1. Click the G3 Stack component, on Configuration Options set G3 Mode of Operation to G3 Stack (ADP + MAC) Hybrid PLC and RF:
      Figure 2-26. Set G3 Mode of Operation
    2. This triggers the G3 Components Auto Activation. For the selected option, 3 Confirmations are required to activate all components, as seen on the following figures:
      Figure 2-27. Auxiliary Services Auto Activation
      Figure 2-28. PAL_Layers Auto Activation
      Figure 2-29. Queue Service Auto Activation
    3. When all components are activated, they appear on the Project Graph:
      Figure 2-30. G3 Components Added
    4. Click the G3 PAL PLC component, on Configuration Options enable PVDD Monitor:
      Figure 2-31. Enable PVDD Monitor
    5. Every other components configuration will use their default values.