1.2 Prerequisites
(Ask a Question)Before you start, perform the following steps:
- Download and install Libero®
SoC on the host PC from the following location:
Libero SoC Documentation
.Important: The latest versions of ModelSim®, Synplify Pro®, and FTDI drivers are included in the Libero SoC installation package.
- Download demo design files from: www.microchip.com/en-us/application-notes/AN4664; and download the PCIe EndPoint design files from: www.microchip.com/en-us/application-notes/AN4597.
- To create Libero Project, see Appendix 3: Running the TCL Script.
- Install the PolarFire® PCIe
Root Port Demo GUI application by running the
setup.exefile available in the design files folder:<$Design_Files_Directory>\mpf_an4664_df\GUI. At the end of the installation, you may be prompted to download and install the FPGA_GUI_Pack, if it is not already available on your system.
- Alternatively, you can manually download and install the Microchip FPGA_GUI_Pack.