9 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the most current publication.

Table 9-1. Revision History
RevisionDateDescription
D09/2025The following is a summary of changes made in the revision D:
C01/2025The following is a summary of the changes made in the revision C:
B06/2024The following is a summary of the changes made in the revision B:
A08/2022The following is a summary of the changes made in the revision A:
7.0—The following is a summary of the changes made in this revision:
  • Updated the document for Libero SoC v2021.2.
  • Added support for PERSTn signal generation.
  • Replaced Figure 1-1 through Figure 1-7.
  • Updated Table 1-2 and Table 2-1.
  • Updated section Design Implementation.
  • AHBtoAXIAPB subsystem is removed from the MiV subsystem.
  • AXI_Interconnect_0 and Core_APB_0 were added in the MiV subsystem.
  • Enabled AXI initiator interface and APB initiator interface on MiV core.
  • Updated the reset structure.
6.0—The following is a summary of the changes made in this revision:
  • Updated the document for Libero SoC v12.6.
  • Removed the references to Libero version numbers.
5.0—The document was updated for Libero SoC v12.0.
4.0—The document was updated for Libero SoC PolarFire v2.3.
3.0—The document was updated for Libero SoC PolarFire v2.2.
2.0—The document was updated for Libero SoC PolarFire v2.1.
1.0—The first publication of this document.