2 Libero Design Flow
(Ask a Question)This chapter describes the Libero design flow of the demo design. The Libero design flow involves the following steps:
- Synthesize
- Place and route
- Verify Timing
- Configure Design Initialization Data and Memories
- Generate Bitstream
- Run PROGRAM Action
Important: To initialize the TCM in PolarFire using the system controller, a local parameter l_cfg_hard_tcm0_en, in the
miv_rv32_subsys_pkg.v file must be changed to 1’b1 prior to synthesis. See the TCM section in the MIV_RV32 Handbook. This user guide can be downloaded from the Libero SoC Catalog.The following figure shows these options in the Design Flow tab.