2.5.4.8 USB_DEVICE_CDC_INIT Structure

C

typedef struct {
  size_t queueSizeRead;
  size_t queueSizeWrite;
  size_t queueSizeSerialStateNotification;
} USB_DEVICE_CDC_INIT;

Summary

USB Device CDC Function Driver Initialization Data Structure

This data structure must be defined for every instance of the CDC function driver. It is passed to the CDC function driver, by the Device Layer, at the time of initialization. The funcDriverInit member of the Device Layer Function Driver registration table entry must point to this data structure for an instance of the CDC function driver.

Members

Members Description
size_t queueSizeRead; Size of the read queue for this instance of the CDC function driver
size_t queueSizeWrite; Size of the write queue for this instance of the CDC function driver
size_t queueSizeSerialStateNotification; Size of the serial state notification queue size

Remarks

The queue sizes that are specified in this data structure are also affected by the USB_DEVICE_CDC_QUEUE_DEPTH_COMBINED configuration macro.