2.3.4.9 USB_DEVICE_AUDIO_RESULT Enumeration
C
typedef enum {
USB_DEVICE_AUDIO_RESULT_OK,
USB_DEVICE_AUDIO_RESULT_ERROR_TRANSFER_QUEUE_FULL,
USB_DEVICE_AUDIO_RESULT_ERROR_INSTANCE_INVALID,
USB_DEVICE_AUDIO_RESULT_ERROR_INSTANCE_NOT_CONFIGURED,
USB_DEVICE_AUDIO_RESULT_ERROR_PARAMETER_INVALID,
USB_DEVICE_AUDIO_RESULT_ERROR_INVALID_INTERFACE_ID,
USB_DEVICE_AUDIO_RESULT_ERROR_INVALID_BUFFER,
USB_DEVICE_AUDIO_RESULT_ERROR_ENDPOINT_HALTED,
USB_DEVICE_AUDIO_RESULT_ERROR_TERMINATED_BY_HOST,
USB_DEVICE_AUDIO_RESULT_ERROR
} USB_DEVICE_AUDIO_RESULT;
Summary
USB Device Audio Function Driver USB Device Audio Result enumeration.
This enumeration lists the possible USB Device Audio Function Driver operation results.
Members
| Members | Description |
| USB_DEVICE_AUDIO_RESULT_OK | The operation was successful |
| USB_DEVICE_AUDIO_RESULT_ERROR_TRANSFER_QUEUE_FULL | The transfer queue is full and no new transfers can be scheduled |
| USB_DEVICE_AUDIO_RESULT_ERROR_INSTANCE_INVALID | The specified instance is not provisioned in the system |
| USB_DEVICE_AUDIO_RESULT_ERROR_INSTANCE_NOT_CONFIGURED | The specified instance is not configured yet |
| USB_DEVICE_AUDIO_RESULT_ERROR_PARAMETER_INVALID | The event handler provided is NULL |
| USB_DEVICE_AUDIO_RESULT_ERROR_INVALID_INTERFACE_ID | Interface number passed to the read or write function is invalid |
| USB_DEVICE_AUDIO_RESULT_ERROR_INVALID_BUFFER | A NULL buffer was specified in the read or write function |
| USB_DEVICE_AUDIO_RESULT_ERROR_ENDPOINT_HALTED | Transfer terminated because host halted the endpoint |
| USB_DEVICE_AUDIO_RESULT_ERROR_TERMINATED_BY_HOST | Transfer terminated by host because of a stall clear |
| USB_DEVICE_AUDIO_RESULT_ERROR | General Error |
Remarks
None.