2.6.4.17 USB_DEVICE_HID_RESULT Enumeration
C
typedef enum {
USB_DEVICE_HID_RESULT_OK,
USB_DEVICE_HID_RESULT_ERROR_TRANSFER_QUEUE_FULL,
USB_DEVICE_HID_RESULT_ERROR_INSTANCE_NOT_CONFIGURED,
USB_DEVICE_HID_RESULT_ERROR_INSTANCE_INVALID,
USB_DEVICE_HID_RESULT_ERROR_TERMINATED_BY_HOST,
USB_DEVICE_HID_RESULT_ERROR
} USB_DEVICE_HID_RESULT;
Summary
USB Device HID Function Driver USB Device HID Result enumeration.
This enumeration lists the possible USB Device HID Function Driver operation results. These values USB Device HID Library functions.
Members
| Members | Description |
| USB_DEVICE_HID_RESULT_OK | The operation was successful |
| USB_DEVICE_HID_RESULT_ERROR_TRANSFER_QUEUE_FULL | The transfer queue is full. No new transfers can be scheduled |
| USB_DEVICE_HID_RESULT_ERROR_INSTANCE_NOT_CONFIGURED | The specified instance is not configured yet |
| USB_DEVICE_HID_RESULT_ERROR_INSTANCE_INVALID | The specified instance is not provisioned in the system |
| USB_DEVICE_HID_RESULT_ERROR_TERMINATED_BY_HOST | Transfer terminated by host because of a stall clear |
| USB_DEVICE_HID_RESULT_ERROR | General Error |
Remarks
None.