3.1.1.3 Automatic Power Switch
The switch between the two power options is controlled by four transistors in an ideal diode configuration, ensuring separation between the two when both are connected. The switch prioritizes power from the wall adapter to maximize power transfer. The following figure shows the automatic power switch topology.
This configuration is not intended to function as a live power switch. Although switching power sources during board operation is generally safe, it can result in a short power drop during transistor commutation and potentially cause a system reset.