3.6.6.1 Command Format (BM70/71 to Host)
|
Value of Parameter (9...10) |
Parameter Description |
Length – 2 Bytes |
|---|---|---|
0xXXXX | HCI-ISDAP command result 0x0000 – Success 0x0001 ... 0xFFFF – Failure | — |
|
Value of Parameter (11...n) |
Parameter Description |
Length = (0xNNNN – 2) Bytes |
|---|---|---|
0xXX | Any data that is associated with a successfully executed command. Note: All HCI-ISDAP
command responses do not always have this parameter
field. Example: For an HCI-ISDAP Read command, the requested memory values read are returned | — |