3.6.3.1 Response Format (BM70/71 to Host)
The following figure and tables illustrate the format and information returned to the host.
|
Value of Parameter (3) |
Parameter Description |
Length – 1 Byte |
|---|---|---|
0xXX | Number of HCI command packets that can be sent to the BM70/71 from the host | — |
|
Value of Parameter (4...5) |
Parameter Description |
Length – 2 Bytes |
|---|---|---|
0xXXXX | HCI Command opcode that is processed by the BM70/71 | Format is little endian |
|
Value of Parameter (6) |
Parameter Description |
Length – 1 Byte |
|---|---|---|
0xXX | For more details on error codes, see Error Code Table Reference | — |