3.6.4.1 Response Format (BM70/71 to Host)
The following figure and tables illustrate the format and information returned to the host.
|
Value of Parameter (3) |
Parameter Description |
Length – 1 Byte |
|---|---|---|
0xXX | 0x00 – Command is pending, but successfully received 0x01 ... 0xFF – For more details on error codes, see Error Code Table Reference. | — |
|
Value of Parameter (4) |
Parameter Description |
Length – 1 Byte |
|---|---|---|
0xXX | Number of HCI command packets that are allowed to be sent to the BM70/71 device by the host. | — |
|
Value of Parameter (5...6) |
Parameter Description |
Length – 2 Bytes |
|---|---|---|
0xXXXX | Opcode of the command that caused this event and is pending completion | Format is little endian |