11.6 Interrupts
I/O Modules have Change Notification interrupts.
| Interrupt Type | Condition | Flag |
|---|---|---|
| Change Notification | Whenever the data to the pin is in accordance with the Change Notification configuration the interrupt is triggered. There is only one flag for each PORT and the exact pin should be checked in the specified registers. | CNxIF |
IO Integrity Module has Error Notification interrupt.
| Interrupt Type | Condition | Flag |
|---|---|---|
| IOIM Interrupt | Whenever the ERR bit is set during the working of IOIM, this interrupt is triggered. There is one interrupt for every instance of the module. | IOIMxIF |