26.4.10.1 Entering Single-Step Mode
Single-Step mode is entered by setting the PTGSSEN bit (PTGCON[9]) =
1.
This bit may only be accessed from a debugging session and will read as
‘0’ at all other times. For example, the following steps can be
used to set PTGSSEN:- In MPLAB® X IDE, program the device to run in Debug mode.
- Pause code execution at any point where PTGSTRT has not been set to
‘
1’. - Add a variable watch for the PTGCON register.
- Using the watch, set the PTGSSEN bit to ‘
1’.
Note: The value of PTGSTRT must be ‘
0’ when setting
the PTGSSEN bit or Single-Step mode will not be entered.Note: Due to the Debug mode restriction, it is not possible to read
PTGSSEN from application code to determine whether Single-Step mode has been entered as
it will always read as ‘
0’.