7.7 getpid Function
Return the process ID of the current process.
Attention: This interface function is
implemented only by MPLAB XC32 C compilers.
Include
<unistd.h>
Prototype
pid_t getpid (void)
Return Value
The pid_t data type is a signed integer type which is capable of
representing a process ID. In the GNU C Library, this is an int.
Remarks
This function is implemented as a stub that must be completed to suit the application.
A process ID uniquely identifies a process only during the lifetime of the process. As a rule of thumb, this means that the process must still be running.
Source File
getpid.c