7.10 lseek Function
Move a file pointer to a specified location.
Include
<unistd.h>
Prototype
long lseek(int handle, long offset, int
origin);
Arguments
handle- handle (file descriptor) referring to an opened file
offset- the number of characters from the origin
origin- the position from which to start the seek
Return Value
Returns the offset, in characters, of the new position from the beginning of the file.
The function returns -1 to indicate an error and sets errno.
Appropriate values might be EBADF or EINVAL.
Remarks
This function is implemented as a stub that must be completed to suit the application.
This helper function is called by the Standard C Library functions
fgetpos(), ftell(), fseek(),
fsetpos and rewind().
<stdio.h>):| Origin | |
|---|---|
SEEK_SET | Beginning of file |
SEEK_CUR | Current position of file pointer |
SEEK_END | End-of-file |
Default Behavior
As distributed, the parameters are passed to the host file system through the simulator. The return value is the value returned by the host file system.
Source File
lseek.c