7.13 sbrk Function
Extend the process’ data space by a given increment.
Include
None
Prototype
void * sbrk(int incr);
Argument
incr- number of characters to increment/decrement
Return Value
Return the start of the new space allocated or -1 for errors.
Remarks
This is a helper function called by the Standard C Library function
malloc().
sbrk() adds incr characters to the break value and changes
the allocated space accordingly. incr can be negative, in which case the
amount of allocated space is decreased.
sbrk() is used to dynamically change the amount of space allocated for the
calling process’s data segment. The change is made by resetting the process’s break value and
allocating the appropriate amount of space. The break value is the address of the first
location beyond the end of the data segment. The amount of allocated space increases as the
break value increases.
Default Behavior
A static variable is used to point to the first free heap location. If adding
incr number of bytes will exceed _eheap,
sbrk() will return -1. Otherwise, the function updates the first free
location on the heap and return a pointer to latest allocated memory.
-Wl,--defsym=_min_heap_size=size MPLAB XC32 option or
-Wl,--heap=size MPLAB XC16 or XC-DSC option is
specified, where size is the desired heap size in
characters. The starting and ending addresses of the heap are reported in variables:
_heap and _eheap, respectively, and which are
declared:extern uint8_t _heap; // heap start
extern uint8_t _eheap; // heap endWhen using MPLAB XC16 or XC-DSC, the linker’s heap size option is the standard way of
controlling heap size, rather than relying on brk() and
sbrk().
See also brk().
Source File
sbrk.c