7.3 brk Function
Set the end of the process’s data space.
Include
None
Prototype
int brk(void * endds);
Argument
endds- pointer to the end of the data segment
Return Value
Returns 0 if successful; otherwise, returns -1.
Remarks
This function is implemented as a stub that must be completed to suit the application.
This helper function is used by the Standard C Library function
malloc().
The brk() function is used to dynamically change the amount of space
allocated for the calling process’s data segment. The change is made by resetting the
process’s break value and allocating the appropriate amount of space. The break value is
the address of the first location beyond the end of the data segment. The amount of
allocated space increases as the break value increases.
Newly allocated space is uninitialized.
Default Behavior
A static variable is used to point to the first free heap location. If the argument
endds is zero, the function sets the variable to the address of the
start of the heap and returns zero. If the argument endds is non-zero
and has a value less than _eheap, the function sets the variable to the
value of endds and returns zero. Otherwise, the variable is unchanged
and the function returns -1.
The argument endds must be within the heap range (see data space memory
map below).
Since the stack is located immediately above the heap, using brk() or
sbrk() has little effect on the size of the dynamic memory pool.
The brk() and sbrk() functions are primarily intended
for use in runtime environments where the stack grows downward and the heap grows
upward.
-Wl,--defsym=_min_heap_size=size MPLAB XC32
option or -Wl,--heap=size MPLAB XC16 or XC-DSC option
is specified, where size is the desired heap size in
characters. The starting and ending addresses of the heap are reported in variables:
_heap and _eheap, respectively, which are
declared:extern uint8_t _heap; // heap start
extern uint8_t _eheap; // heap endWhen using MPLAB XC16 or XC-DSC, the linker’s heap size option is the standard way of
controlling heap size, rather than relying on brk() and
sbrk().
Source File
brk.c