7.5 creat Function
Obsolete function
Attention: This interface function is
implemented only by MPLAB XC32 C compilers.
Include
<fcntl.h>
Prototype
int creat(const char * filename, mode_t mode)
Arguments
filename- name of the file to open
mode- the file permission bits
Return Value
On success, creat returns a file descriptor to the open file; on
error it returns -1 and should set errno to indicate the
error.
Remarks
This function is implemented as a stub that must be completed to suit the application.
Opens the specified filename for writing, truncating to length zero, and creating it if it does not exist.
Source File
creat.c