7.12 read Function
Read data from a file.
Include
<unistd.h>
Prototype
int read(int handle, void *buffer, unsigned int
len);
Arguments
handle- handle (file descriptor) referring to an opened file
buffer- points to the storage location for read data
len- the maximum number of characters to read
Return Value
This function should be implemented to returns the number of characters read, which may
be less than len if there are fewer than len
characters left in the file or if the file was opened in text mode, in which case, each
carriage return-linefeed (CR-LF) pair is replaced with a single linefeed character. Only
the single linefeed character is counted in the return value. The replacement does not
affect the file pointer. If the function tries to read at end-of-file, it returns 0. If
the handle is invalid, or the file is not open for reading or the file is locked, the
function returns -1 and errno is set to indicate the kind of error.
Appropriate values may be EBADF or EINVAL, among
others.
Remarks
This function is implemented as a stub that must be completed to suit the application.
This helper function is called by the Standard C Library functions
fgetc(), fgets(), fread() and
gets().
Default Behavior
As distributed, the parameters are passed to the host file system through the simulator. The return value is the value returned by the host file system.
Source File
read.c