7.14 unlink Function
Low level command to remove a file link.
Include
<unistd.h>
Prototype
int unlink(const char * name);
Argument
name- file to be removed
Return Value
Returns zero if successful and -1 to signify an error.
Remarks
This function is implemented as a stub that must be completed to suit the application.
This function is not provided by default and is required for remove and
rename. This function deletes a link between a filename and the
file contents. The contents are also deleted when the last link is destroyed. A file may
have multiple links to it if the link function has been used.
Source File
unlink.c