7.1 _exit Function
Terminate program execution.
Attention: This interface function is not
implemented by MPLAB XC8 C compilers.
Include
<unistd.h>
Prototype
void _exit(int status);
Argument
status- exit status
Remarks
This function is implemented as a stub that must be completed to suit the application.
This is a helper function called by the exit() Standard C Library
function.
Default Behavior
As distributed, this function flushes stdout and terminates. The
parameter status is the same as that passed to the exit() standard C
library function.
Source File
_exit.c