7.9 link Function
Create a new file.
Include
<unistd.h>
Prototype
int link(const char * existing, const char * new);
Arguments
existing- filename from which to link
new- destination filename of link
Return Value
Zero is returned to indicate success, and -1 is returned to indicate an error condition.
Remarks
This function is implemented as a stub that must be completed to suit the application.
This function is not provided by default. Its purpose, in a file system, is to create a
new filename, new, which contains the same data as the file named
existing. The errno object should also be set on
error. This function is used by rename.
Source File
link.c