3.8.9 mcHalI_DirectionButtonState
C
/* Get direction button state */
bool mcHalI_DirectionButtonState( void )
Summary
Retrieve the state of the direction button.
Description
This function is used to read the status of the direction button configured for motor control in the Harmony QSpin GUI.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| void | None. |
Returns
- True: Returns true if the button is pressed.
- False: Returns false if the button is not pressed.
Example
/* Get direction button state */
mcHalI_DirectionButtonState();
Remarks
None.