3.8.1 mcHalI_StartStopButtonState
C
/* Get start-stop button state */
bool mcHalI_StartStopButtonState( void )
Summary
Retrieve the state of the start-stop button.
Description
This function is used to read the status of the start-stop button configured for motor control in the Harmony QSpin GUI.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| void | None. |
Returns
- True: Returns true if the button is pressed.
- False: Returns false if the button is not pressed.
Example
/* Get start-stop button state */
mcHal_StartStopButtonState();
Remarks
None.