3.4.11 tmcRpc_Input_s Struct
C
/* Data structure for Rotor Position Calculation (RPC) module input ports */
typedef struct
{
uint16_t encPulseCount; /* Encoder pulse count value */
<#if __PROCESSOR?matches(".*PIC32MK.*") == true>
int16_t encVelocityCount; /* Difference in encoder counts between cycles */
</#if>
}tmcRpc_Input_s;
Summary
RPC module input parameter structure.
Description
This structure holds the input parameters for the Rotor Position Calculation (RPC) module, including the current encoder pulse count value and difference in encoder counts between cycles.
Remarks
Refer the generated header file for the exact typedef signature.