3.22.3 Shared VLAN Learning Configuration
Shared VLAN Learning (SVL) allows for frames that are initially classified to a particular VLAN (based on Port VLAN ID or VLAN tag information) to be bridged on a shared VLAN. In SVL, two or more VLANs are grouped to share common source address information in the MAC table. The common entry in the MAC table is identified by a Filter ID (FID).
Command Syntax:
svl fid <fid> vlan <vlan_list>
no svl fid { <fid_list> | all }Argument | Description | |
Parameter |
| The FID must be a number between 1 and 63. |
| List of VLANs mapped into FID. Individual elements are separated by commas and ranges are specified with a dash. | |
| List of one, more or all FIDs. | |
Default | N.A | |
Mode | Global Configuration mode | |
Usage | Create SVL. To change all VIDs currently mapped to the FID back to being independent (IVL), use the ‘no’ version of the command. | |
Example | Example 1: Let VID 2, 4 and 20-200 map to the same shared VLAN, 13. Example 2: Let all VLANs currently mapped to FID 7 and 10 return to Independent VLAN Learning (IVL). | |