3.23.1 Port to Group Configuration
Use this command to configure switch ports to use a given VLAN Translation Mapping group.
Command Syntax:
switchport vlan mapping <gid>Argument | Description | |
Parameter |
| Group id. Integer value from 1 to 8. |
Default | N.A | |
Mode | Port List Interface mode | |
Usage | Enable all VLAN Translation mappings of that group (if any) on the selected switch port. | |
Example | Example 1: Configure port 2 to use the VLAN mapping group 1. | |