3.12.2 Link Event Configuration
Use this command to configure the frame error, error-symbol period, and frame-seconds summary event window, as well as the threshold that trigger a link event.
Command Syntax:
link-oam link-monitor frame { [ window <error_window> ] [ threshold <error_threshold> ] }
link-oam link-monitor frame-seconds { [ window <error_window> ] [ threshold <error_threshold> ] }
link-oam link-monitor symbol-period { [ window <error_window> ] [ threshold <error_threshold> ] }Argument | Description | |
Parameter |
| Duration of the monitoring period in terms of seconds. |
| Number of permissible errors frames in the period defined by the error window. | |
Default | N.A | |
Mode | Port List Interface mode | |
Usage | N.A | |
Example | Example 1: Configure frame error event window 10sec and threshold 3 that trigger an error-frame link event on port 2. | |