3.14.4 CIST/MSTI Port Configuration
Use this command to configure the STP CIST/MSTI aggregated and normal ports parameters.
Command Syntax:
spanning-tree aggregation spanning-tree mst <instance> cost { <cost> | auto }
spanning-tree mst <instance> priority <prio>
spanning-tree edge spanning-tree auto-edge spanning-tree restricted-role
spanning-tree restricted-tcn
spanning-tree bpdu-guard
spanning-tree link-type { point-to-point | shared | auto }Argument | Description | |
Parameter |
| STP bridge instance. Must be set to 0 (zero) for the CIST and to a value between 1 and 7 for MSTI. |
| Port priority must be divisible by 16. Supported values are 0/16/32/48/64/80/96/112/128/144/160/176/192/208/224/240. The default value is 128. | |
| The Auto setting sets the path cost as appropriate by the physical link speed, using the 802.1D recommended values. A user-defined value can be entered. Valid values are in the range of 1–200000000. | |
Default | N.A | |
Mode | STP Aggregation mode and Port List Interface mode | |
Usage | Configure STP CIST/MSTI aggregated and normal ports parameters. To revert to default, use the ‘no’ version of the command. | |
Example | Example 1: Configure the CIST aggregated port priority 32. Example 2: Configure the CIST port 2 priority 64 with auto edge disabled. | |