3.14.3 MSTI Priority Configuration
Use this command to configure the STP MSTI bridge instance priority.
Command Syntax:
spanning-tree mst <instance> priority <prio>Argument | Description | |
Parameter |
| STP bridge instance. Must be 0 (zero) for CIST, and 1–7 for MSTI. |
| Bridge Priority. Supported values are 0-61440. Only values divisible by 4096 are allowed. For example, 4096, 8192, 12288, and so on. The default value is 32768. | |
Default | N.A | |
Mode | Global Configuration mode | |
Usage | Configure STP system settings. To revert to the default, use the ‘no’ version of the command. | |
Example | Example 1: Configure STP MSTI2 Priority12288. | |