3.13.1 Loop Protection General Settings
Use this command to configure Loop protection general parameters.
Command Syntax:
loop-protect loop-protect transmit-time <t>
loop-protect shutdown-time <t>Argument | Description | |
Parameter |
| Interval between each loop protection PDU sent on each port. Valid values are 1–10 seconds. The default value is 5. |
| Period for which the port is kept disabled when a loop is detected. Valid values 0–604800 seconds (7 days). A value of 0 keeps the port disabled until the next device restart. The default value is 180. | |
Default | N.A | |
Mode | Global Configuration mode | |
Usage | Enable/disable Loop protection (globally) and configure Loop protection parameters. To reset to the default, use the ‘no’ version of the command. | |
Example | Example 1: Enable Loop protection and set transmit time to 8 seconds, shutdown time to 500 seconds. | |