12 Reference Circuit
This section provides the reference schematics of IS2062GM, IS2064GM, IS2064S and IS2064B used in a stereo headset application.
The following figures illustrate the IS2062GM reference schematics for the stereo headset application.
Note: All ESD diodes in these schematics are
reserved for testing.
The following figures illustrate the IS2064GM (IS2064GM-012/IS2064GM-0L3) reference
schematics for the stereo headset application.
Note: The AOHPR, AOHPL and AOHPM pins shown in the
following schematic are not applicable for IS2064GM-0L3 as there is no analog audio output
pin. These pins must be left unconnected.
Note: All ESD diodes in these schematics are
reserved for testing.
The following figures illustrate the IS2064S reference schematics for a stereo headset application.
Note: All EDS diodes in these schematics are
reserved for testing and can be removed if ESD is passed without adding it.
The following figures illustrate the IS2064B reference schematics for the stereo headset application.
Note: All ESD diodes in
these schematics are reserved for testing and can be removed if ESD is passed without adding
it.