1 Device Overview
The IS2062/64 SoC integrates:
- Bluetooth 5.0 dual-mode radio transceiver
- Power Management Unit (PMU)
- Microcontroller (MCU)
- Audio codec
- Crystal oscillator
- 32-bit DSP
- Flash (IS2062GM/64GM)
- EEPROM
The IS2062/64 SoC is configured using an UI tool.
Note: The UI tool is a Windows® based
configuration utility tool, which is available for download from the Microchip website at
www.microchip.com/wwwproducts/en/IS2062 and www.microchip.com/wwwproducts/en/IS2064.
The following figure illustrates the block diagram of the IS2062/64 SoC.
Note:
- IS2062GM
- IS2064GM
- IS2064S
- IS2064B