1.3.5.4.27 CL_NULL_PMlmeSetRequest Function

C

void CL_NULL_MlmeSetRequest
(
    uint16_t pibAttrib,
    void *pibValue,
    uint8_t pibSize
);

Summary

Set a new value for a given PIB attribute of the MAC layer.

Description

This routine is used to set a new value for a given PIB attribute of the MAC layer.

Precondition

The CL_NULL_Initialize routine must have been called before.

Parameters

ParametersDescription
pibAttribPIB attribute
pibValuePIB attribute value
pibSizePIB attribute value size

Returns

None.

Example

uint8_t bandSearchTime = 25;
CL_NULL_MlmeSetRequest(PIB_MAC_MIN_BAND_SEARCH_TIME, &bandSearchTime, sizeof(bandSearchTime);

Remarks

The result of the request is returned in the confirm callback.