1.3.5.4.21 CL_NULL_MlmeMpPromoteRequest Function

C

void CL_NULL_MlmeMpPromoteRequest
(                
    uint8_t *eui48,
    uint8_t bcnMode,
    uint16_t pch
);

Summary

Request to trigger the promotion process in a Service Node (Terminal or Switch) in a medium (PLC or RF) different from the one the node is connected to the network.

Description

This routine is used to request to trigger the promotion process in a Service Node (Terminal or Switch) in a medium (PLC or RF) different from the one the node is connected to the network.

Precondition

The CL_NULL_Initialize routine must have been called before.

Parameters

ParametersDescription
eui48Pointer to the address of the node to be promoted (NULL in Service Node)
bcnModeBeacon PDU modulation scheme
pchPhysical channel

Returns

None.

Example

uint8_t eui48[6];
memset(eui48, 0x12, 6);

CL_NULL_MlmeMpPromoteRequest(eui48, 0, 16);

Remarks

The result of the request is returned in the confirm callback.

This primitive only applies in PRIME v1.4.