1.3.5.4.13 CL_NULL_PlmeSleepRequest Function
C
void CL_NULL_PlmeSleepRequest(uint16_t pch);
Summary
Request a suspension of all present activities of the PHY layer.
Description
This routine is used to request a suspension of all present activities of the PHY layer.
Precondition
The CL_NULL_Initialize routine must have been called before.
Parameters
| Parameters | Description |
|---|---|
| pch | Physical channel (v1.4) |
Returns
None.
Example
CL_NULL_PlmeSleepRequest(16);
Remarks
The result of the request is returned in the confirm callback.