1.3.5.4.14 CL_NULL_PlmeResumeRequest Function

C

void CL_NULL_PlmeResumeRequest(uint16_t pch);

Summary

Request to resume all suspended activities of the PHY layer.

Description

This routine is used to request to resume all suspended activities of the PHY layer.

Precondition

The CL_NULL_Initialize routine must have been called before.

Parameters

ParametersDescription
pchPhysical channel (v1.4)

Returns

None.

Example

CL_NULL_PlmeResumeRequest(16);

Remarks

The result of the request is returned in the confirm callback.