1.3.5.4.16 CL_NULL_PlmeGetRequest Function

C

void CL_NULL_PlmeGetRequest
(
    uint16_t pibAttrib,
    uint16_t pch
);

Summary

Request information about a given PIB attribute of the PHY layer.

Description

This routine is used to request information about a given PIB attribute of the PHY layer.

Precondition

The CL_NULL_Initialize routine must have been called before.

Parameters

ParametersDescription
pibAttribPIB attribute
pchPhysical channel (v1.4)

Returns

None.

Example

CL_NULL_PlmeGetRequest(PIB_PHY_STATS_RX_TOTAL_COUNT, 16);

Remarks

The result of the request is returned in the confirm callback.