5.1.1.1 BDB Commissioning APIs
The following table lists the BDB API related to commissioning, detailing its function prototype and functionality.
| Function Prototype | Description |
|---|---|
void BDB_SetBdbNodeIsOnANetwork(bool onNetwork) | Set the bdbNodeIsOnANetwork status |
bool BDB_GetBdbNodeIsOnANetwork(void) | Get the bdbNodeIsOnANetwork status |
| The API actively calculates the Cyclic Redundancy Check (CRC) for the install code and compares it with the provided CRC. Then, it derives the link key using the Symmetric-Key Security Protocol Advanced Encryption Standard (SSP AES) and sets this key in the APS key pair set. |
bool BDB_InvokeCommissioning(BDB_InvokeCommissioningReq_t *req) | The commissioning API invokes the commissioning based on the given information in the request structure. |
void BDB_ResetVia_TouchlinkCluster(ResetTargetCallback_t pfcallback) | Resets the target device to factory defaults using touch-link commissioning cluster |
void BDB_SetInstallCodeUsage(bool useInstallCode) | Sets the install code usage at the trust center |
void BDB_SetNodeJoinTimeout(uint8_t timeOutInSec) | Sets the node join time-out |
void BDB_SetTCLKExchangeMethod(uint8_t exchangeMethod) | Sets the TCLK exchange method BDB attribute |
void BDB_SetTCLKRetryMaxAttempts(uint8_t attempts) | Sets the TCLK retry max attempts BDB attribute |
void BDB_SetTCRequireKeyExchange(bool requireKeyExchange) | Sets the trust center require key change or not of the joining device |
void BDB_SetToulinkRole(bool initiator) | Sets the touch-link role |
void BDB_ResetIB(void) | Resets the BDB information base/attributes |