5.2.1 Oscillator Options
MPLAB X IDE requires information about your target oscillator to simulate device execution and support the stopwatch feature. For more on the Stopwatch, see Using the Stopwatch.
| Instruction Frequency (Fcyc) (Note 1,2) | Enter the instruction execution
frequency value. The units are specified below.
|
| Frequency In (Note 1,2) | Specify the units for the instruction frequency above, either MHz, KHz or Hz. |
| RC Oscillator Frequency | For devices that have an internal RC oscillator, enter the RC oscillator frequency value. See the device data sheet for the range of possible values. |
| RC Oscillator Frequency In | Specify the units for the RC oscillator frequency above, either MHz, KHz or Hz. |
| Auxiliary Clock Frequency (Faux) | For devices that have an auxiliary oscillator, enter the auxiliary clock frequency value. See the device data sheet for the range of possible values. |
| Auxiliary Frequency In | Specify the units for the auxiliary frequency above, either MHz, KHz or Hz. |
| Note 1: These values
will also be used to set certain fields in the Stopwatch. Note 2: Configuration bit settings will have no effect on processor speed, e.g., if using x4 PLL, simulator will run at processor frequency, not 4 times processor frequency. | |